Part Number: DP83867IRPAP-EVM
Other Parts Discussed in Thread: DP83867IR
Hello,
I'm using DP83867IR.
For the debugging purpose, I tried MII loopback mode (Near-end loopback).
However when the signal loops back, the RX_ER signal was always asserted.
The MAC could receive the looped back frame by suppressing the RX_ER signal (setting register GPIO_MUX_CTRL2[0:3] = 1000 (constant "0")).
The speed was 10 and 100 Mbps. Both speed setting resulted in same.
My question is...
What is conceivable cause of the RX_ER in this case?
Best regards,
Tsunokawa