Part Number: TUSB1044
Hi,
We are using TUSB1044 for cable re-drive application. We want to preliminary testing of part with FPGA SerDes signals (these are not USB) before we start with actual testing with USB signals.
We are generating PRBS sequence in the FPGA and providing it to one of the channels of TUSB1044 and checking to see whether we can get the output on the other side of TUSB1044. We are not observing any signal on the other side of TUSB1044 and tried with all combinations of switch settings. In one setting, we had seen LFPS signaling generated from USB exerciser observed on other side of TUSB with DIR0 = 1 and SLP_S0#=1.
1. Whether TUSB1044 allow any generic SerDes signal instead of USB/DP?
2. Is the device protocol aware?
3. We are using GPIO mode and switch settings are DIR0 = 1 and SLP_S0# = 1 rest all are 0.
Thanks,
Naveen