Part Number: TUSB8020B
Hi,
Recently issues starting to appear on TUSB8020B design I inherited. The issue seems to be the same on all boards - 24MHz oscillator does not start. I verified the voltage power up and the 3ms reset mentioned in the datasheet, but everything seems to be OK.
The crystal used is ECS-240-20-30B-TR. Changing the crystal on several boards does not help, but what always helps is to exchange the TUSB8020B chip.
Is there anything particular what the chip is sensitive to?
Is there anything I could measure to advance a little bit more?
What is the crystal pins input capacitance?
There are two vias between each crystal pin and the input pin, could this be the source of issues?
Thank you
Regards
Petr