To whom this may concern,
I have been able to view the pattern generated from the DS90UB954 deserializer on a csi-2 output, however when I attempt to generate the pattern using the same indirect access register settings on the ds90ub953 i don't get any frames on the csi-2 interface. Is there any additional configuration, apart from fpd-III forwarding on the deserializer, required on either of the serializer or deserializer in order to get this working?