Part Number: ONET4211LD
Hello Team,
The ONET4211LD should work between 155 Mbps up to 4.25 Gbps
Would the ONET4211LD works at 1-100MHz?
If not, what prevents it?
If yes, which specification from the datasheet may be more affected from the lower bit rate?
Thanks,
SunSet