This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS6126: pls help to check if HD3SS6126RUAR support SGMII single switch?

Part Number: HD3SS6126


Dears pls help to check if HD3SS6126RUAR support SGMII single switch?

  • HD3SS6126 will work with SGMII, please make sure you are able to meet HD3SS6126 control and differential pin signaling voltage requirement.

    Control pins requirements
    • VIH from 2 V to VDD
    • VIL from –0.1 V to 0.8 V

    Differential pairs requirements:
    • VI/O_Diff from 0 V to 1.8 Vp-p
    • VI/O_CM from 0 V to 2 V

    Thanks
    David