Part Number: TUSB8020B
Hi Sirs,
Sorry to bother you.
Our application is carrier board.
Upstream will connect to NVIDIA TX1/TX2 (USB3.0/2.0), Two downstream connect to USB3.0 Type A connector,
The circle is highlight which need to confirm
We also need to know GANGED/SMBA2/ HS_UP and FULLPWRMGMTz/ SMBA1/SS_UP pin function.
Could you help explain it?
When will it be needed? If it is not used, could it be floating?