Part Number: DS80PCI402
We are using the part for a design of a PCI-e Add in Card (Host Bus Adapter) for NVMe storage.
We have been told that there can be up to 10db of insertion loss to our card and possibly another 2db on the card.
On the downstream side we have a 70CM Cable to our device which has an additional 6-8" of etch. It has been characterized as having 15db loss.
I am determining the configuration settings for the redriver to provide the cleanest eye pattern at both the root and end point positions.
the 12db host path transmits into the Port B inputs and then redrives out the cable to the device.
The Device transmitter through the cable goes into the Port A receivers. and is then driven through the 12db path to the root.
can you help me determine the best configuration settings to accomplish this?
Thanks in advance.
Robert Bentley