Part Number: TPS2549
Other Parts Discussed in Thread: TPS2546
Dear Team,
My customer is considering to use TPS2549 at USB Port of their module.
But they require very low Rds_on on high-side switch. Then, they are thinking the following application.
[Very low Rds_on High-side Switch Device] ------(VBUS)
+
[TPS2549 for USB Charging Port Controller] -----(D+ & D-)
When operation Port type of the TPS2549 is set only “Dedicated Charging Port (DCP) Mode”, the above application is OK, right?
When operation Port type is set “CDP-SDP Auto Switch Mode”, the above application is not OK, because there is OUT discharge operation under CDP-SDP Auto Switch mode, right?
Under the CDP-SDP Auto Switch Mode, when they want to use the external very low Rds_on High-side Switch Device, how should they do?
Thank you.
Best Regards,
Koshi Ninomiya