Part Number: DP83822I
Hi apps team,
Could you give me comments on the following customer questions?
Q1. The customer wants to replace PHY-A to DP83822I(PHY-B). But for the register 0x0001, bit [6], SMI preamble suppression, the default value is different from PHY-A (which value is '0') and PHY-B (which value is '1'). In that case, what restriction will happen for the link partner with DP83822 caused by the default value difference? Or there is not any restriction no matter what the default value is?
Q2. For the register 0x0018, bit[9,10], in the case that the customer sets 5Hz (100ms on-time, 100ms off-time) for example, and, LED_0 is set by BLINK for TX/RX Activity, what happen on the on-time if TX/RX activity happens during the on-time at the blink? For example, does taking the on-time longer than 100ms happen?
Q3. In the case that DP83822 is progressing reset sequence, what happen if receiving signal from the link partner?
Q4. To confirm, is there any product specification, which requires software reset after hardware reset is completed, not described on the datasheet?
Thank you for your support.
Best regards,
Takeshi Sasaki