Part Number: TMDS171
Hi
Our customer evaluates at some abnormal condition such as ON/OFF operation of power supply (kind of temporary power down).
And they found a unknown phenomenon.
If the power OFF / ON test is repeated, an event that the TMDS signal is not output from the TMDS 171 will occur about 1/100 times.
Since there are several questions, please confirm the following question.
1) Datasheet: There is a sequence gauge in "8.3.2 Operation Timing" on page 23, but is there a regulation of ON → OFF → ON sequence? (Image as shown on the bellow)
* For example,since the power supply voltage does not falls if it is not taken for more than a few ms from OFF to ON, there is a possibility of malfunction etc.
2) Since the TMDS signal is not output, it may be in the standby mode.
What is the condition that TMDS is not output in the state of power ON and TMDS input?
3) In order to investigate the cause mentioned above, are there any registers for reference when checking register setting?
And I have another question that is not related above question.Regarding the pull up resistor at control pin, the resistor is 65kohm as it mentioned at the datasheet.
However the cusotmer connect the pull up resistor (65kohm) from 3.3V supply rail to the control pin then the voltage of the controll pin will be 2.5V.
The min voltage of VIH is 2.6V as it defined at datasheet. The voltage of the pins is lower than the specification.
Is this correct?
Best Regards,
Koji Hamamoto