Part Number: TIC12400
Dear team,
My customer want to know how operate after reset. please review below and let me know your opinion.
- Vs : 24V
- The customer want to use IN1 ~ IN7 to current sink not source port (reset -> select current sink -> wetting current 2mA -> port Enable)
- After reset , default value of Input port is disable / sourcing / no wetting current.
- After reset, Even though IN_EN_1~7 register value is 0h(disable), Can IN1~IN7 ports operate as a sourcing ports? The customer are concerned that 24V Vs could give damage to other device if IN1~IN7 operates as a sourcing port though IN_EN_1~7 is 0h(disable).
Thank you.