Part Number: TPS65987D
Hi, Team,
Do you have a register which can configure 2.7V Divider3 Mode Advertisement from 1.2V Mode Advertisement? A customer would like to use 2.7V Divider3 Mode, but the system cannot detect 2.7V Divider3 Mode adapter. The D+/D- voltage is less than 1.5V, so I think the system is working as 1.2V Mode Advertisement.
Best Regards,
Satoshi Yone