This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: DS90UB954-Q1 csi clock no out put

Part Number: DS90UB954-Q1


We are using ti 954/953 serdes, but we can't make the image output normally. 

we use 954/953 sync mode by STP cable with below settings, but the mipi csi output from 954 is abnormal, 

we can we only get the csi data output but without the csi clock. 

please help to check what's wrong, 

thanks

BRs

johnny

static UINT8 ti954_reset[]=
{
0x01, 0x03, // Reset
0xff, 0x0a, // delay 0-0xfe
0xff, 0xff // end loop
};

static UINT8 ti954_init_ch1[]=
{
0x4c, 0x01, // enable reg write for RX0 port
0x58, 0x5d, // enable I2C pass through 0x5e<=not work
0x5c, ALIAS_ID_DESER_CH1, // set Remote SER Alias
0x5d, IDC_ID_BRV0200_CH1, // device_slave_id
0x65, ALIAS_ID_SENSOR_CH1, // device_slave_Alias_id
0xff, 0xff // end loop
};

static UINT8 ti954_init_ch2[]=
{
0x4c, 0x01, // enable reg write for R0 port
0x58, 0x5d,//0x9a,//0x58, // enable I2C pass through 0x5e<=not work
0x5c, ALIAS_ID_DESER_CH2, // set SER Alias
0x5d, IDC_ID_BRV0200_CH2, // device_slave_id
0x65, ALIAS_ID_SENSOR_CH2, // device_slave_Alias_id
0xff, 0xff // end loop
};

static UINT8 ti954_enable[]=
{
0x33, 0x03, // CSI_CTL Enable CSI output
0xff, 0x64, // delay
0x20, 0x20, // Forwarding control enable R0 Port
0xff, 0xf0, // delay
0x0c, 0x01, // Enable Port 0 Receiver
0xff, 0xff // end loop
};
//--------------------------------------------------------------
static UINT8 ti953_init[]=
{
0x07, 0x14, // N CLKOUT_CTRL1
0xff, 0x64, // delay
0x0e, 0xf0, // gpio output enable
0x0d, 0x0c, // set SEN_RSTn, PWDN
0xff, 0x0a, // delay
0x0d, 0x08, // sensor reset
0xff, 0x64, // delay
0x0d, 0x0c, // set SEN_RSTn, PWDN
0xff, 0x0a, // delay
0x0b, 0x28, // set UB953 I2C rate
0x0c, 0x28, //
0x02, 0x73, // Set the continue mode sjq important
0xff, 0x10, // delay
0x1c, 0x3f, // ALARM_CSI_EN
0x1e, 0x03, // ALARM_BC_EN
0x49, 0x28, // BC_CTRL
0xff, 0xff // end loop
};


Initial steps,
1. ti954_reset
2. ti954_init
3. ti953_init
4. Sensor Init
5. ti954_enable