Part Number: TUSB1002A
Hi,
The routing topology for customer is PCH-->TUSB1002A-->USB3 Mux-->TypeC Connector.
Now we know the trace length from PCH to TypeC connector is 6 inch, and the differential insertion loss (@ 5GHz) is -2.2dB from the USB3 Mux. May I know if it's ok to implement TUSB1002A at a 4 inch distance to PCH, and 2 inch distance to type-c connector? If this is not good, what would be your proposal?
Thanks!
Antony