Part Number: SN65DP159
Hello,
My customer has some questions about SN65DP159.
[Q1]
When I2C_EN/PIN = 1, the termination for HDMI TX set with 0Bh[4:3].
In this case, Is the automatically select the termination impedance feature disabled ?
[Q2]
There is no TX_TERM_CTL pin for RSB package.
When I2C_EN_PIN = 0 in RSB package, is TX_TERM_CTL NC (automatically select the termination impedance feature is enabled) ?
Best Regards,
Hiroshi Katsunaga