Part Number: DP83822I
Hello,
Our customer use the DP83822.
They configure the LED_0 and LED_1 as Mode2.
So they connect resistor to CRS pin as pull-up:13kohm and pull-down 1.96kohm.
They use the DP83822 with 100BASE-TX Full duplex.
It should set the LED_0 pin as Mode3. So it should be connected resistor to LED_0 pin
as pull-up 6.2kohm and pull-down 1.96kohm.
In this configuration, does the LED_0 pin recognize the pull-down resistor and
configured as an active high driver?
*Because the condition of our network is bad, I'm sorry if the posts have been doubled.
Best Regards,
Naoki Aoyama