Part Number: SN65MLVD047
Other Parts Discussed in Thread: SN65LVDT388A, , DS90LV047A, SN65LVDS391
What is the load current and ground current for SN65MLVD047PW M-LVDS QUAD line driver?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65MLVD047
Other Parts Discussed in Thread: SN65LVDT388A, , DS90LV047A, SN65LVDS391
What is the load current and ground current for SN65MLVD047PW M-LVDS QUAD line driver?
Dear Yaser
We are planning to loopback SN65MLVD047PW driver to SN65LVDT388ADBT receiver with 100 Ohm termination. Does the interface work?
Else, please suggest me loopback circuit with the same components.
Regards
Srikanth Kacchu
Dear Yaser
You are correct. I am connecting output of SN65MLVD047 to SN65LVDT388A with external 100 Ohm termination. Since SN65LVDT388A having internal 100 ohm termination. Together makes 50 ohm termination at the output of SN65MLVD047.
Reason for selecting SN65MLVD047 M-LVDS driver is to driver 4 receivers. I am not sure about a normal driver can able to load 4 receivers.
Regards
Srikanth Kacchu
Dear Yaser
While interfacing one board with another board, each output of SN65MLVD047of one board will drive 4 receiver inputs in another board. This is one point.
Next point is, I have SN65MLVD047 driver and SN65LVDT388A receiver in my board. To validate these devices I planned to connect one driver output to one receiver input only. The same circuit is drawn and attached here. I have external termination of 100 ohm at driver output and the receiver has 100 ohm internal termination. Together making 50 ohm at M-LVDS driver output as recommended. So, please check and clarify.
Regards
Srikanth KacchuLVDS Loopback.pdf