Hi Team,
I have a customer who is using the TUSB8041 but have no need for the charging features since all 4 ports will be operated in SDP(USB2.0) mode. I want to verify some of the pins whether they should be pulled-up, pulled-down, or leave floating.
I was referring to this post where it was suggested to leave the PWRCTL pins floating rather than pulling them down so I want to verify some of the other pins.
1) PWRMGMT_EN#: pulled up to 3.3V
2) PWRCTL_POL
3) GANGED
4) AUTO_EN
Thanks for the help in advance and best regards,
Jerry