This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: Unused Pins when Charging Features are not needed

Part Number: TUSB8041

Hi Team,

I have a customer who is using the TUSB8041 but have no need for the charging features since all 4 ports will be operated in SDP(USB2.0) mode.  I want to verify some of the pins whether they should be pulled-up, pulled-down, or leave floating. 

I was referring to this post where it was suggested to leave the PWRCTL pins floating rather than pulling them down so I want to verify some of the other pins.

1) PWRMGMT_EN#: pulled up to 3.3V 

2) PWRCTL_POL

3) GANGED

4) AUTO_EN

Thanks for the help in advance and best regards,

Jerry