Other Parts Discussed in Thread: SN75DP139
Hi ,
My product has two HDMI, using TI solution SN75DP139 chips.
I have a problem , In 594MHz and 891MHz , it is over EMI limit value. The over comes from HDMI port.
I try to slove the problem , ex. adjust VSadj from 3.9K to 4.02Kohm and change CMC 90ohm to 120ohm.
But the results are limited,EMI still exceeds.
So , Can you recommand solution to slove the EMI issue from HDMI port ?