Part Number: TPS65987D
Hi, everyone,
I'm designing using TPS65987D.
But when we attach 2.7V divider mode charger, it won't work properly.
For example, if we attach charger (divider 1),
D+ 2.0V -> about 0.8V
D- 2.7V -> about 1.3V
so I wonder if there's something wrong with TPS65987D & surrounding settings.
Now, I have 2 questions:
1) Are their settings are correct so that we can use BC1.2 & Apple charger mode?
2) Are there any registers concerned about this problem ?
Our settings are as follows:
***** 0x29 Port Control *****
[31:30] Charger Detect Enable ... 11b BC1.2 and proprietary detection enabled)
[28:26] Charger Advertise Enable ... 110b DCP auto mode 1)
[24] Resitror 15k Present ... 0b 15kOhm resistor not present
***** 0x5c I/O Config *****
GPIO #18:
[400:407] Mapped Event: Disabled
GPIO #19:
Multiplexing for GPIO 19 pin: Pin Multiplexed to GPIO
[408:415] Disabled
**********
Best Regards,