Part Number: DP83848I
Hello Team,
I'm having problems to get the DP83848 working at 10Mbits while at 100Mits it looks ok.
At 100Mbits the performance are slightly lower than expected so some errors may still occur but it is working
testing the board with ipconfig at 10Mbit:
RX packets:105176 errors:104547 dropped:0 overruns:0 frame:15627
basically all errors.
The error occurs with point to point connection with the end device, as well with a switch in between.
So it does not look related to signal amplitude issue.
the register settings are for forced 10Mbit-HD:
eth0: 10 Mbit, half duplex, link ok
registers for MII PHY 0:
0000 784d 2000 5c90 01e1 0000 000f 2801
0000 0000 0000 0000 0000 0000 0000 0000
0003 0000 3c00 0000 0000 0000 0100 0001
0000 8021 0804 0000 0000 6011 242f 0000
product info: vendor 08:00:17, model 9 rev 0
basic mode: 10 Mbit, half duplex
basic status: link ok
capabilities: 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
advertising: 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
For forced 100Mbit-HD:
eth0: 100 Mbit, half duplex, link ok
registers for MII PHY 0:
2000 784d 2000 5c90 01e1 0000 000d 2801
0000 0000 0000 0000 0000 0000 0000 0000
0601 0000 3000 0000 0000 0000 0100 0001
0000 8021 0804 0000 0000 6011 08be 0000
product info: vendor 08:00:17, model 9 rev 0
basic mode: 100 Mbit, half duplex
basic status: link ok
capabilities: 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
advertising: 100baseTx-FD 100baseTx-HD 10baseT-FD 10baseT-HD
Do you see any problems?
thanks
SunSet