Dear Technical Support Team,
Is it possible to change Pin Control Mode or SMBUS Mode during operation?
In my image,
When ENSMB is changed from 0 to 1, pins of EQ and DEM is disable and PMbus is enable.
Register setting of EQ/DEM is changed default.
When ENSMB is changed from 1 to 0, pin of EQ and DEM is enable and PMbus is disable.
Is it correct operation?
I think that Common pin like DEM_S1/SCL、DEM_S0/SDA are very complicated when changed them during operation.
User should change correct external register(I2C pull up and 4Level)
Best Regards,
ttd