Part Number: TUSB320
Other Parts Discussed in Thread: , TUSB422
TUSB320 USB Type-C™ Configuration Channel Logic and Port Control
What’s difference between ST (STUSB1602) and yours(TUSB320IRWBR)?
Why are your IC almost 2X as expensive as theirs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Judy,
The ST device is a Type-C controller with USB PD while the TUSB320I is a Type-C controller. In regards to pricing, I do not see anything wrong after checking the different sites. Could you point me to where you obtained pricing. I would actually suggest to use the TUSB320LAI which is our latest gen.
Do you need USB PD for your application? If so, then I would suggest the TUSB422.
Regards,
Charlie