Part Number: SN65HVD1785
We have developed a system that employs the SN65HVD1785 to interface between several modules. Our modules are powered from a 24VDC source. The 24VDC source can be common(shared) or independently supplied to the modules. Where the 24V is shared this implies a common ground to the modules.
My question is, when the units are powered from separate 24VDC, do I have to supply a dedicated 0V line linking the modules.
In other words when interfacing with SN65HVD1785, do we need to supply a dedicated 0V line.