This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65981: Pulse outputs for CC1 and CC2 have suddenly dissappeared !!

Part Number: TPS65981

I have a second rev design using the TPS65981ABIRTQR.

I built 9 boards.  All worked, then eventually, they failed.

I now have one board working, 8 boards not.

Rev A boards still work and output correct pulses.

I have tracked the problem down to the fact that the PD controller (TPS65981ABIRTQR) is no longer outputting the CC1 and CC2 pulses required for USB 3.0 cable (and cable direction) detection.

What could disable these pulses ?