Part Number: TPS25810
Other Parts Discussed in Thread: TPS2561A
Dears,
I am developing an USB type-C battery charger, I'd like to use TPS25810 but I need to understand if TPS25810 is compliance with IEC62680-1-1
many thanks
regards
Roberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roberto,
This is currently being looked into. An answer will be posted when available.
Hi Darwin,
yes, you are on right, my solution is 15W (5V/3A).
So, as I understood, I can use TPS25810 for this application (charger for USB type C only in DCP mode (Dedicated Charging Port)).
I hope that TPS2561A could be used for another similar application (15W) but dedicated for USB type A.
Many thanks in advance for your feed-back.
Best regards,
Roberto