Part Number: TUSB9261
Hi Team,
I wanted to use TUSB9261 in one of the designs.
The application is that I need USB2.0-to SATA conversion. The TUSB9261 will be connected to external HDD over SATA interface.
My question is suppose I want to take the backup of data from external HDD over USB interface , can the below block diagram work.
During normal operation, USB2.0 lines from the processor is selected to the TUSB9261 chip and when backup is required, USB3.0 will be connected to the TUSB9261 chip. IS ther any code/firmware for the above scenario. Please update if this application is possible.