Part Number: TLK10031
Other Parts Discussed in Thread: TLK10034
Hi,
Once link training has completed, the 10G-KR data path is enable but the link is lost on one of the test boards when the power supply is turned on and off repeatedly.
Looking at the difference between OK and NG, it seems that the eye pattern was fail, didn't open enough, so there seems to be a problem with the parameters obtained by link training.
Could you please tell me how to improve this issue ?
The important register settings are shown as below.
HS_SERDES_CONTROL_1 (register: 0x0002) (device address: 0x1E) ---> 0x831C
HS_SERDES_CONTROL_2 (register: 0x0003) (device address: 0x1E) ---> 0xA848
HS_SERDES_CONTROL_3 (register: 0x0004) (device address: 0x1E) ---> 0x7500
The addresses with different register values for OK and NG are as below.
HS_STATUS_1 (register: 0x0016) (default: 0x0000) (device address: 0x1E)
KR_FEC_C_COUNT_1 (register = 0x00AC) (default = 0x0000) (device address: 0x01)
KR_VS_RX_CTC_INSERT_COUNT (register = 0x8017) (default = 0xFFFD)
Best regards,
Kato