Part Number: TCAN1042-Q1
Dear, Sir.
My customer is evalating TCAN1042-Q1 now. They have an experience to apply
NXP/TJA1042, so asking a question comapring that. Please give your advice.
1. TCAN1042-Q1 has VIO or NC pin (#5). Does it mean this pin is originally connected
to the internal circuit & supply Volatge of IO such as 3.3V when the voltage traslation
is needed? Sorry I would like to double-confirm.
2. TJA1042 has SPLIT pin, but TCAN1042-Q1 doesn't have.
Is it possible to provide the testing data of Bit Eror Rate using TCAN1042-Q1?
Best Regards,
H. Sakai