Part Number: TUSB542
Hi,
I have noticed that there is no requirement of power supply decoupling and input caps on the TUSB542 datasheet. The example application doesn't show them either. Pin assignment of VDD18 (Pin 5) is not a convenient location to place decoupling and input caps. Does that mean this device doesn't require caps at the 1.8V rail? Is there any reason for that?
I have also run the.bxl file to get PCB symbol and footprint. I have noticed that the schematic symbol have RX pair and TX on swapped. On datasheet the pin top view shows RX(+/-) on Pin 18/17; TX(+/-) on Pin 15/14. But on the schematic symbol, Pin 18/17 are named as Tx(+/-); 15/14 as Rx(+/-). The direction of each pair on the symbol matches the description in the datasheet though. I just want to confirm which is right. And you may want to correct the name on the PCB symbol file.
Thanks,