Hello all,
i am using stm3240g-eval development board and together with dp83848C and I am trying to bring up the Ethernet module.
I was unable to send and receive data using the MII interface.
the following configurations has been set.
MII mode
PHY address - 0x01
Auto.negotiation - Enabled
speed - 100Mbps
with above configuration, in basic mode status register bit 5 is not set.
is there any internal clock of 25MHZ to the dp83848C??.
Kindly help me overcome the above problems.
Best Regards,
Siva