Part Number: PCA9306
Hello,
I am using this to Translate the level of the I2C, in the My master device I2C is 2.5V and Slave device I2C is 1.8V.
Previous instance i have connected Master device I2C in Port A at 1.8V and Slave Device I2C in Port B at 3.3V.
But Now i need to connect in Reverse way, Which mean in Port A i need to connect the Slave device and Port B i need ti connect the Master Device?, Can any resolve this issues. In the Datasheet its always specified from Port A to Port B and not Vice versa?