This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS26LV32AT: On hold the last state output

Part Number: DS26LV32AT


Hi All,

We have used this IC in our application.IC part number : DS26LV32ATMX/NOPB

our Problem:

The output pins of this IC is holding the the last state output until we give the next input.

If input HIGH - output HIGH

Next If open the inuput- it is holding the last state (HIGH)

If given input is LOW - output is LOW

Next If open the inuput- it is holding the last state (LOW)

Please help us how to solve this issue.

We are using Rt = 120ohm, but we haven't use any pullup or pulldown at the input pins (As datasheet recomend)

Regards,

G.Prabhakaran