Part Number: TUSB422
I am currently in layout for a TUSB422-based design and the via for the INT_N ball is the only laser-drilled via in the whole design. My design does not need VCONN support and the VCONN ball is currently unconnected. Is there anything that would preclude routing the INT_N line through the VCONN pad and avoiding the laser-drilled via? Leakage current into/from VCONN when VCONN_EN is disabled is not specified.