Part Number: DP83867E
I am using DP83867E , when connected to a gigabit switch the speed seems fine.
But when same is connected to a 100 Mbps switch , it slows down drastically . One ping cmd takes around 400 ms.
Is there any specific settings that need to be taken care in its linux device tree config ?
Is it related to rx, tx internal delays?
Or the issue can be in hardware designing?
What are appropriate steps to debug the issue?
Thanks.