This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Internally Generated FrameSync

Expert 3040 points
Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP

Hi Team, 

Customer wants to use FrameSync Signal for Sensor using internal FrameSync mode.

They were trying to set along with the following register settings. However, problem is this mode didn't work.

Is it possible to check the following setting if there is something wrong? 

BC_FREQ_SELECT is set to 50Mbps.

-----------------------------------------------------------------------------------------

#Register set on 953;

0x0E: 0x87

0x0D: 0x80

#Register set on 954:

#define DES's BC_GPIOs to framesync signal

0x6F:0xA8

#configure framesync for internal generation

0x18:0x45

#fs_high_time

0x19:0x00

0x1A:0x18

#fs_low_time

0x1B:0x6C

0x1C:0x68

-----------------------------------------------------------------------------------------

Regards, NY