Part Number: DP83848C
Hello,
I was wondering if anyone could elaborate on the following.
Document www.ti.com/.../snla088a.pdf specifies recommendations for configuring transformerless operation.
Specifically, it states
"IEEE compliance testing was performed on the transformerless interface with both straight and crossover cables. The results showed compliance for critical 100 Mb/s mode parameters (jitter, tx/rx return loss, Vod). Other IEEE tests, which are designed to simulate worst-case cable loading, did not pass, thus supporting the recommendation to use short distance configurations in non-typical transformerless applications"
Is it possible to find out what specific tests failed? It recommends applications for cables less than 1 meter in length. What sort of results might one expect to see if longer cables were to be used?
Best regards,