Part Number: TLK10232
Dear TI developers,
We have product using TLK10232, we want to bring up on new platform.
Somehow we cannot get 1G-KX link up properly, we want to inquiry with you in detail.
The previous platform has a GE switch with 2 ports connect to TLK10232 HS;
Channel A is 10G-KX and Channel B is 1G-KX.
Based on the attachment, we can use the 'init sequence' + 'setup loopback on same port' to get TLK10232 link up on 10G-KR;
and using 'init sequence' + '1G-KX setting' + 'setup loopback on same port' to get TLK10232 link up on 1G-KX.
The new platform is using Intel CPU w/ X552 10 GbE Backplane connect to TLK10232 HS.
We want to using the same sequence as old platform to get link up,
We are able to get 10G-KR link up, but failed on 1G-KX portion.
Since the new platform, the HS media is changed,
Do you suggest to modify the setting for 0x1e.[2-5], which are related to HS_SERDES_CONTROL ?
If yes, I think the Intel x552 10GbE is common component,
Do you have the experience for configure these HS_SERDES_CONTROL?
Thank you.
Alan