Part Number: TPS65987D
Other Parts Discussed in Thread: TIDA-050014
I would like to power TPS65987D from VBUS1, since there is no system 3.3V available in my design. Should VIN_3V3 be left as no connect in that case, or is a decoupling cap needed on that input?
I also wanted to clarify the current limiting capability of TPS65987D. According to the datasheet, the power switch has overcurrent protection at Iocp, which is 10A, but I did not see a configurable overcurrent limit lower than that when operating as a sink. There is a firmware configurable overcurrent clamp, Iocc, but only when operating as a source (see Section 8.3.3.1.1). Do I need an external fuse, then, if I want to implement a lower OCP limit (e.g., 1A or 1.5A) for PD sink?
Thanks,
Brian Angiel