This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1EVM: where I can find Script ovt_1280_1080_30fps_REMOTE.py for DS90UB954 ?

Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: ALP

Where I can find python script for 

ovt_1920_1080_30fps_REMOTE.py

P954_A0_RX0_CSI_Enable.py

P954_SETUP_A0_4G.py

954_A0_Init.py, 

954_A0_REFCLK.py, 

954_A0_SetupCSI.py

FPD-link_Assist.py

Thanks!

Fei Zhu

  • Fei,
    We have some scripts available in the ALP installation folder under "PreDefScripts". You can refer to the 954 device folder for the OVT and generic imager setup scripts. The A0* scripts are no longer needed when using the production silicon.
  • Palaniappan,
    Thanks for quick response. I installed Analog LaunchPAD V1.57.00010 version. I can't find the "PreDefScripts" in the installation folder. I had "profiles" folder, which has DS90UB954 folder under it, but inside the DS90UB954 folder, I only had ChanelRegistersGUI.py, DS90UB954_GUI.py, DS90UB954_Lib.py, InternalRegistersGUI.py, RemoteRegisteresGUI.py in it. no any OVT and generic imager setup script for it.
    I also checked the DS90UB953 filder, same structure, no OVT and imager setup script inside.
    By the way, how can I use " WriteI2C(0xB0,0x14) " in the ALP Script windows? since the WriteI2C is not defined.
    Thanks lot!
  • Fei,
    Under the Analog LaunchPAD v1.57.0010 you should see a "PreDefScripts" folder in addition to "Profiles". This PreDefScripts has sub-folders for all the FPD-Link devices, and you will see the scripts under DS90UB954 sub-folder.
    Please make sure that the ALP-PROFILE-UPDATE from the ALP page (http://www.ti.com/tool/alp) is installed on your machine.