This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH948-Q1: PWM output for back light control from DS90UH948-Q1.

Part Number: DS90UH948-Q1


Hi,

We are using DS90UH948-Q1 for converting FPD to Dual LVDS.

We need to control back light driver IC using PWM signal.

As DS90UH948-Q1 does not have any dedicated PWM output pin, can we configure one of the GPIOs of DS90UH948-Q1 for generating PWM?

Requirement of PWM signal for LED driver IC is

PWM Dimming Frequency - 50Hz to 50kHz

PWM Dimming Minimum Duty Cycle - FDimming = 200Hz  Typical value 0.2%

PWM Dimming Minimum Pulse-Width -  Max 5 μs.

If we can't  configure GPIO in to PWM , Please suggest any PWM generator IC which controller by I2C of DS90UH948-Q1.

Regards,

Francy Babu