Part Number: SCANSTA112
Hi,
I am designing a board where I need to multiplex 32 JTAG devices(FPGAs). As per the plan the devices are divided it into 8 chains with 4 devices each. 7 chains are connected to each of the LSPs of the STA112 and for the remaining 1 chain, a separate JTAG programming connector will be used. STA112 will be in transparent stitcher mode.
I have the following questions related to the design:
1) What is the difference in the affect of TRSTb on STA112 and affect of RESET on STA112?
2) In transparent stitcher mode, does TRSTb reset the STA112 logic? Is there some way to mask it in this mode?
3) Can we use the TLR_TRST and TLR_TRST6 in transparent stitcher mode to drive the TRST of the unselected LSPs?
4) Is there a limit on the number of devices that can be connected to each LSP port? Can we connect 8 devices? If we could eliminate that one extra JTAG connector it would be great.
Shruti