Part Number: TPS65987D
Tool/software: Code Composer Studio
HI TI,
In the program, I encountered some problems and wanted to be clarified. As described below:
(PWR confg. host only , Output ability 5V@3A 12V@2A )
<Item/sheet --- > Q&A>
1). High/Low Voltage Warning --> When the option is turned on, Warning message will appear in ?
2). High/low Voltage Warning Level --> already has Over voltage Protection Trip Point, What is the difference between the High Voltage Warning Level and Over voltage Protection Trip Point?
3). Set UVP Debounce --> What is the Debounce mean here? Function is?
4). Programmable voltage(power) thershold --> My HW configuration does not control external FET through GPIO, And my biggest output capacity is 24W, how should I do this?
5). Auto Negotiate sink min required power --> According to my output ability, how to set?
5). PD3 Configuration Register sheet --> Support xxxxx message, Will these messages appear in?
6). peek current (duty cycle) -- > What is the duty mean here?
7). Tx Source Capabilities Extende sheet --> <A> Regarding the power part, if I use the internal MOSFET how should I set it? <B> Is this page setting mosfet controlled by GPIO? <C> peek current 1,2,3 What is the location of the corresponding HW?
8). Battery Design capacity / Battery Last Full Charge Capacity / Battery Type --> If not used, Value default is?
BR,