This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1064: TUSB1064 Tjmax parameter,

Part Number: TUSB1064

hi sir:

please help provide TUSB1064 Tjmax parameter, we can't find it on datesheet.
customer needs to do thermal simulation.

thanks

  • Hermes

    Max junction temperature for commercial TUSB1064 is 110C. Max junction temperature for industrial TUSB1064 is 125C.


    (Junction temperature) Tj = Ta + (P * Junction-to-ambient thermal resistance)

    Ta is the ambient temperature
    P is dissipation power which is available in table 6.5.

    Thanks
    David