Other Parts Discussed in Thread: SN54LS673, SN54HC595, SN74HC595B
Hello,
I'm looking for an SPI I/O Expander IC that is MIL-temp rated (-55C to +105C or better). I've found the SN54LS673 but the power consumption is a bit high and it's an old part. I couldn't find an updated version of the component. We'd be mainly using the expander to control some FETs and analog switches. Here are some things I need it to do:
- Serial Inputs
- Minimum of 8-bit parallel output
- Needs to be double-buffered ("shift and store")
- Must power up in a known state (with a reset pin that clears the output latch)
- Wide VCC range (at least 3.3V to 5V)
- Military temp (-55C to +105C or better)
I know there are some I2C I/O Expanders out there but that may be a little slow for my application. Does anyone have any suggestions on a component(s) to use?