Part Number: DS90UA101-Q1
Other Parts Discussed in Thread: DS90UA102-Q1
Hi all
Would you mind if we ask DS90UA101-Q1?
There is the description on the data sheet P24;
"If the number of audio channels is more than 8, DS90UA101-Q1/DS90UA102-Q1 can easily support multiplexed data with additional devices to multiplex and de-multiplex the data.
The number of channels multiplexed on each data line must be selected as a power of 2, for example, 2/ 4/ 8."
We would like to configure 16 audio channels, is it possible to configure it using one DS90UA101-Q1 device?
Does "with additional devices to multiplex and de-multiplex the data." mean that it requires to use two DS90UA101-Q1 devices for 16 audio channels?
Could you give us the configuration In case of 16 audio channels?
Kind regards,
Hirotaka Matsumoto