Part Number: DS125BR800
While creating a PCIe x8 reDriver Card, i want to use two DS125BR800 chips: one for TX and second one for RX channels.
Both chips should read Equalization Info from on-board EEPROM. According Application Report SNLA228 (Page 4), to eliminate conflicts with EEPROM, i should connect ALL_DONE of the first DS125BR800 with READ_EN of the second DS125BR800.
The question is: should I connect ALL_DONE with READ_EN directly, or should i use a transistor to create a transition from high to low (Page 4 of the Datasheet DS125BR800 says, that "When using an External EEPROM, a transition from high to low starts the load from the external EEPROM")?
Thank you for response.