Hi,
I want to know the difference of operation by setting Output Mode.
If we select "0" = 10G-KR operation, How waveform the device output?
and If we select "1" = normal operation, How waveform the device output?
Best regards,
Shimizu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to know the difference of operation by setting Output Mode.
If we select "0" = 10G-KR operation, How waveform the device output?
and If we select "1" = normal operation, How waveform the device output?
Best regards,
Shimizu
Hi,
Setting "0" = 10G-KR produces a more linear drive characteristic. The low frequency voltage gain is reduced to ~ 1.3x. This makes the output amplitude dependent on the input amplitude.
Setting "1" = normal operation produces a limiting drive characteristic. There is significant voltage gain through the device in this mode. The output amplitude is set using VOD/DEM controls.
Note: For this register bit in 0x10 to take effect, it is necessary to also program the following registers.
Write 0x06 = 18'h
Write 0x08 = 04'h
Regards,
Lee
Hi Lee,
Thank you for your previous reply.
I have a question about your answer.
"The low frequency voltage gain is reduced to ~ 1.3x." in your answer.
I think "~ 1.3x" shows to increase.
Could you let me know more detail about this mean, please?
This device has De-emphasis function.
I could understand the part of "The low frequency voltage gain is reduced".
Best regards,
Shimizu
Hi Shimizu,
When the output is in normal mode and there is a 100mV input amplitude, the output level will be determined by the VOD setting. Example VOD setting = Level 5, output amplitude = 1V.
When the output is in 10G-KR mode and there is a 100mV input amplitude, the output level is mostly determined by the input amplitude. Example VOD setting = Level 5, output amplitude will be ~ 100mV x 1.3 = 130mV.
Enabling an output setting with De-emphasis will further reduce the low frequency output amplitude.
Regards,
Lee